While working in Teamcenter 11.2 with NX10.0.3, does the Manufacturing Resource Library (MRL) reserve any Teamcenter attribute classification values that should not be touched?
Solution
MRL does not use any positive attribute IDs.
The range of attributes IDs from -999 up to 999 is reserved for some internal classification attributes. These attributes are not listed in the attribute dictionary. These reserved values have nothing to do with MRL. This is a fixed state by the Classification application. This block includes internal attributes that can be queried by API. Attribute blocks are reserved to prevent conflict.
It is recommended to use attributes and also Key-LOVs in a specific range:
Recommended Range Attribute IDs: 100000 to 110000
Recommended Range Key-LOV IDs: -100000 to -110000 (Unfortunately, all Key-LOV IDs are negative numbers.)
Only positive attribute IDs should be used. The minimum number is 1000. The recommendation is to pick numbers in the range of 100000 to 110000.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: TC_MFG
Ref: 001-7946852