NX
NXOpen Language Bindings that Work with the run_journal.exe Utility
2019-05-01T12:00:06Z
NX OpenNX System Administration
Summary
Details
What journals work with run_journal.exe?
Solution
The run_journal.exe utility program requires the user to set the all of the same environment variables that are required to start an interactive session of NX.
For best results, we suggest that you use an NX Command Prompt window launched from the NX Tools menu. NX12 and later should be installed on the Certified Windows 10 OS so the NX Command Prompt will be available.
The journals that work with this function are Visual Basic, C# and Python.
Block/UI Interface Stylers
Knowledge Fusion
Menuscript
NX Open - All Languages
NX Open Python
Open for C/C++
Open for CAE
Open for GRIP
Open for Java
Pre-NX6 UI Styler
SNAP
UDO