NX Simulation Parse Errors are Reported when using Heidenhain ISO Mode

2019-08-20T12:20:08Z
NX for Manufacturing

Summary


Details

Can the Heidenhain ISO mode be used when simulating using one of the sample simulation machines provided by NX?



Solution

The Heidenhain ISO mode is not supported in the out-of-the-box Heidenhain MCF file. Though the NC code for this output is similar to the Fanuc the MCF file would require edits in order to prevent the reported parse errors.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1876
Function: ISV

Ref: 001-7737235

KB Article ID# PL8010361

Contents

SummaryDetails

Associated Components

Manufacturing ISV Robotic Machining