NX10 is not printing line widths correctly

2019-05-15T15:30:50Z

Summary


Details

NX10 will not print line widths correctly



Solution

 The default line width scale factors used by the 'File-->Print' command were 
changed for NX10.0.


For NX10.0, the default scale factors range from 1.0 to 3.0. 
The default scale factor settings were changed to match default pixel width 
settings, which were also changed in NX10.0. 


To modify the scale factors, modify the settings in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Gateway' and highlight 'Printing (Windows Only)'. 
3. Select the 'General' tab. 
 Currently, the Width Scale Factors range from 1.0 to 3.0 in NX10.0. 
4. Modify the Width Scale Factors as desired. 
 To set the same settings as previously in NX9.0, note the following: 
 The settings for 'Thin Width Scale Factor', 'Normal Width Scale Factor' 
 and 'Thick Width Scale Factor' did not change between NX9 and NX10. 
 However, the remaining 9 Width Scale Factors fields 
 in NX9 were 1.0, 2.0, 3.0, 4.0, 5.0, 6.0, 7.0, 8.0, 9.0 (top to bottom). 
5. OK the Customer Defaults dialog. 
6. Re-start NX for the changes to take effect.


NOTE: The Width Factors can also be modified directly on the Print dialog. 
1. In the Settings group, in the 'Width' list, highlight the desired 
 width to be modified. 
2. Enter the new scale factor in the 'Scale Factor' field.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V10.0
Function: DISPLAY

Ref: 001-7308785

KB Article ID# PL8010347

Contents

SummaryDetails

Associated Components