Modifying the snap distance when extending oridinate dimensions

2019-05-15T17:05:33Z

Summary


Details

When dragging an existing ordinate dimension to a new location, there seems to 
be a "snapping" distance for the new location of the dimension. The snapping 
distance that the cursor is jumping is too large and is causing the 
dimension to be placed incorrectly.


How can this snapping distance or snapping point be modified?



Solution

 NOTE: If a snapping distance is not desired, hold down the ALT key on the 
keyboard while dragging the ordinate dimension to allow the the dimension to 
be relocated freely without snapping points.


If a snapping distance is desired, after creating an Ordinate dimension, the 
'Spacing' setting for Margins can be modified. 
1. Hover the cursor over the ORDINATE origin. 
 This is the origin that the ordinate dimension is using, usually labeled 
 "ORDINATE1" or "ORDINATE2", etc. 
2. MB3-->Edit. 
3. In the Ordinate Dimension dialog, select the 'Margins' button. 
4. Change the 'Spacing' value to something very small, like .1. 
 NOTE: The value needs to be greater than 0.0. 
5. Exit the dialog.


Now drag the dimensions to a new location. The "snapping" distance should be 
much smaller giving better control over the placement of the ordinate 
dimension.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V7.5
Function: DIMENSION

Ref: 001-7179827

KB Article ID# PL8010344

Contents

SummaryDetails

Associated Components