nxtopvdirect translator exhibiting PER_PART behavior for a MONOLITHIC setting

2019-05-01T12:46:43Z

Summary


Details

User has set StructureOption to MONOLITHIC in the tessUG.config file, but Dispatcher is still generating "per part" assemblies. Why is this option not working?



Solution

There is information in the underlying command "run_ugtopv.bat" that says:


-honour_structure Honours the structureOption value in the .config file. 
 This produces JT files in the format previously generated 
 by the ugtojt translator. This allows support for 
 MONOLITHIC and FULL_SHATTER structure options. 
 Warning: This option will fully load the assembly and 
 will therefore use more memory.The files produced 
 can not be used for interoperation.


To get monolithic JT assembly files from this Dispatcher translator, you will 
need to manually edit the ugtopvdirect script. Namely change this line: 
"%UGII_BASE_DIR%\PVTRANS\run_ugtopv.bat" -u=gtacdba -p=gtacdba -g=dba 
-config="%UGII_CONFIG_FILE%" -noupdate "-pim=yes" %3 %4 %5 %6 %7 %8 %9


To this: 
"%UGII_BASE_DIR%\PVTRANS\run_ugtopv.bat" -u=gtacdba -p=gtacdba -g=dba 
-config="%UGII_CONFIG_FILE%" -noupdate "-pim=yes" -honour_structure %3 %4 %5 
%6 %7 %8 %9 
(note addition of "-honour_structure")



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V12.0
Function: NX_JT

Ref: 001-7922121

KB Article ID# PL8010342

Contents

SummaryDetails

Associated Components