Simcenter 3D Solutions Managing Material data - Modifying material data

2019-05-08T17:27:02Z
Simcenter 3D

Summary


Details

--------------- 

How to modify the material data from a table field to a constant value in NX 

10?

Solution

 When editing material data and a table file is being referenced, the wrench 

icon (edit) will be visible on the far right. Left click the wrench and a 

pull down menu will appear. Select the "Formula" option, which will convert 

the table reference to a forumla that references a table. Delete the entire 

formula from the field and type a constant to replace it. Verify the values 

using the Preview Solver Syntax tool on the Manage Materials form.

Notes

KB Article ID# PL8010339

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow