NX Export CAE simulation to JT2Go, but loads do not show up.

2019-10-28T08:52:54Z
NX for Design

Summary


Details

When exporting the SIM file within Advanced simulation to JT. It does not show (all) loads and constraints in JT2Go.


In the JT, the "assembly" tree is missing the loads and constraints, and also these are not displayed in the graphics area. While other objects are shown, like the Simulation Objects.



Solution

When exporting a simulation to JT, it will export all that is shown in the current model and as shown in the graphics are. 
If you have hidden for example the loads, these are also not exported to the JT file, and cannot be shown. 
So check the "check boxes" in front of the loads, constraints and simulation objects, etc. If they are grey, they will not be exported to the JT.


Make sure you turn them on (red check mark), in order to have them exported.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: TRANSLATOR
Version: V12.0
Function: NX_JT

Ref: 001-8299162

KB Article ID# PL8010335

Contents

SummaryDetails

Associated Components

CAD Translators