Customizing the NX Ribbon interface and when placing icons on the TOP and BOTTOM border bars, the icons are snapping to the center of the border bars and not on the left side.
How to make them start from the left side?
Solution
When NX is set to 'File -> Preferences -> User Interface -> Layout -> Ribbon Bar Options: Slim Ribbon Style', the icons will automatically be centered on the TOP and BOTTOM ribbon bars.

Unchecking to turn off the option "Slim Ribbon Style" will allow icons to start on the left side of border bars.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 10_1507
Product: NX
Application: GATEWAY
Version: V1847
Function: PREFERENCES
Ref: 001-7812726