How to install NX with a HWKEY (Dongle) License?

2020-03-27T10:49:43Z

Summary


Details

NX installation with dongle license (HOSTID=UG_HWKEY_ID=xxxx) and Rainbow SuperPro dongle.



Solution

1. You must have a Rainbow SuperPro dongle and an accordingly license file like the example below:


PACKAGE P1 ugslmd 30.0 COMPONENTS="P1_3d_to_2d_flattener \ 
 P1_assemblies P1_c_p_p_runtime P1_drafting P1_dxf_to_ug \ 
 P1_dxfdwg P1_features_modeling P1_free_form_modeling \ 
 P1_gateway P1_grip_execute P1_iges P1_nx_freeform_1 \ 
 P1_nx_freeform_2 P1_pstudio_cons P1_pv_ugdatagenerator \ 
 P1_solid_modeling P1_step_ap203 P1_step_ap214 P1_ufunc_execute \ 
 P1_ug_smart_models P1_ug_to_dxf P1_ugopen_menuscript" \ 
 OPTIONS=SUITE ck=174 SIGN="182C 196B 699A A775 2EE7 9D24 55CF \ 
 A647 D153 0E3C 9FA4 AE9C E18B 09D2 842E 0383 784A CB30 F5F6 \ 
 7711 83D4 0F2A A103 1116 BB82 1D0C 6B07 36D0 F66B 3709" 
FEATURE P1 ugslmd 30.0 permanent uncounted HOSTID=UG_HWKEY_ID=2185 \ 
 user_info=P1 ck=0 SIGN="0C7B 4250 B779 12F6 1781 6429 16D5 \ 
 D634 AA66 2D40 F626 78F8 9C31 1B9C 82EE 107B 57EF CD81 155F \ 
 ECF8 86C3 B0D3 4134 97A8 5140 FC80 0761 6867 6379 E527" 
FEATURE gateway_id ugslmd 30.0 permanent uncounted HOSTID=DEMO ck=205 \ 
 SIGN="131B CC57 B8BF BFBB 6D66 C087 C8A1 566C BFAB B850 FBA1 \ 
 2A44 FD48 496F AB11 1F51 D202 E72F 36B0 FB64 4BF4 F935 5ADB \ 
 F316 A29D FCF7 CEF3 75D6 4E1A 8467" 
FEATURE server_id ugslmd 30.0 permanent uncounted \ 
 VENDOR_STRING="1081218 - XX XXX/XXX XXXX" HOSTID=ANY \ 
 user_info=K3VMMIARI2 ISSUER=SIEMENS ck=164 SIGN="14DF 4008 \ 
 A325 71A5 AEA7 61EF 1894 7AA3 3A70 489D A436 DE3F C305 6B62 \ 
 0E39 0513 4BEE 27D4 DED2 004B 8BA9 E95F 48C2 CC81 9251 B859 \ 
 550A FCB0 52C5 79B0"


Makes sure to find the string "HOSTID=UG_HWKEY_ID=" in it.


2. Create a folder (e.g. C:\NX_License) and copy the license file in this folder. 
    Give the license a meaningful name (e.g. NX10_Dongle.lic)


3. Install the NX software. 

Please note:
This type of licensing is a so called "Stand Alone" installation and no license server is needed to install. Skip this step in the launch.exe.

During the installation process you will be prompted for the license. Browse to the license file C:\NX_License\NX10_Dongle.lic 
-> the variable SPLM_LICENSE_SERVER=C:\NX_License\NX10_Dongle.lic will be created automatically.


4. After the installation navigate to the folder ${UGII_BASE_DIR}\UGFLEXLM and execute the file 
   "sentinel_installer.exe". 
   This will install the Sentinel software for the communication between NX and the dongle. 
   Please note: The dongle must not plugged in.


5. Download the program "Sentinel Advanced Medic" from 
    http://www.safenet-inc.com/support-downloads/sentinel-drivers/ 
    With this program you can check if the Sentinel software has installed properly 
    and the dongle will be detected.


6. Plug-in the dongle and execute the "Sam1.3.1.exe". 
    In the upcoming window click on "Troubleshoot". The "Basic Checks" should running successfully.


7. Bundle selection: 
    Execute the file "LicensingTool.exe" in the folder ${UGII_BASE_DIR}\UGFLEXLM. 
    In the upcoming window click on "Bundle Settings" and choose the desired bundle.


8. Start NX. The program should coming up successfully and without errors.



Notes and References

nx_install_wnt.pdf in the subfolder "DOCS" of the download of NX.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V10.0
Function: WNT_INSTALL

Ref: 001-8261634

KB Article ID# PL8010320

Contents

SummaryDetails

Associated Components