'Trim and Extend' no longer has a Distance option

2019-05-15T15:30:25Z

Summary


Details

The 'Trim and Extend' command in NX10 no longer has the 'By Distance' option, 
like it did in NX9.



Solution

 This functionality is now available in NX10 by using the 'Extend Sheet' 
command. To access this function: 
1. Select in the Menu, 'Insert-->Trim-->Extend Sheet'. 
2. On the Extend Sheet dialog, select the Edge to extend. 
3. Under the Limit group in the dialog, set the Limit to 'Offset'. 
4. Set the Offset to the distance to offset the edge. 
5. OK the dialog. 
There's also a drag handle available in the work area on the selected edge.



Notes and References

See the NX Help documentation for additional information about the options 
available under the Settings group in the dialog.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V10.0
Function: FREE_FORM_MODEL

Ref: 001-7897212

KB Article ID# PL8010319

Contents

SummaryDetails

Associated Components