NX Cannot select a view for View Dependent Edit

2019-05-13T20:09:27Z
NX for Design

Summary


Details

--------------- 
It is not possible to select a detail view for a View Dependent Edit.



Solution



You must convert to an independent view first.


Documentation on Covert to Independent View:


Convert to Independent View


If you want to make independent edits to the detail view, you must first 
disassociate the detail view from the parent view. You can do this by 
right-clicking the detail view boundary or its corresponding node under the 
parent view node in the Part Navigator, and then choosing Convert to 
Independent View.


When you break the association to a parent view, detail views can be treated 
like any other view. You can do the following to the detail view:


Change the view settings.


Add, remove, and edit curves in the detail view.


Add view dependent edits.


Create additional detail views.


Associated detail views appear as a node beneath the parent view node, while 
non-associated detail views appear as specific view nodes in the Part 
Navigator. 


Note - Once you disassociate a detail view from its parent view, you can not 
reassociate it. Style and view dependent edits made in the parent view do not 
appear in a disassociated detail view. However, view boundary changes made to 
a disassociated detail view are reflected in the parent view



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 001-6976987

KB Article ID# PL8010310

Contents

SummaryDetails

Associated Components

Drafting