How to use keyboard accelerators to change dimension decimal places.

2019-07-31T14:01:05Z

Summary


Details

In NX 10 it is no longer possible to change the number of decimal places, when creating or editing a Drafting dimension, by using the number keys on the keyboard. This was possible in NX 8.5.



Solution

Due to the changes made to the Drafting dimension user interface it is no longer possible to support 'single key' keyboard accelerators, similar to the behavior in NX 8.5.

However, the user can change the number of decimal places when creating or editing dimensions by using a combination of the 'Alt' + '0-6' keys. This was implemented in NX 10.0.2.


Note also that the keyboard accelerators for selecting a dimensions 'Appended Text' fields are 'Alt' + 'Direction Arrow' keys.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V10.0.2
Function: ANNOTATION

Ref: 001-7698268

KB Article ID# PL8010297

Contents

SummaryDetails

Associated Components