Reference geometry is not highlighted for PMI dimensions in TcVis

2019-05-08T09:45:27Z

Summary


Details

--------------- 
In NX we created PMI dimensions and saved it to JT. 
We set in JT Configuration file the following PMI-options to "true": 
 activateNotePMI = true 
 activateCsysPMI = true 
 activateWeldPMI = true 
 activateGDTPMI = true 
 activateSymbolPMI = true 
 activateFosPMI = true 
 activateDimPMI = true 
 activateFcfPMI = true 
 activateDatumPMI = true


We can see these PMI Dimensions in Teamcenter PortalViewer. 
But if we select (highlight) PMI dimension, reference geometry (edges or 
faces) is not highlighted.


In NX reference geometry is highlighted. 
Why can't we see it in JT?



Solution

 Reference geometry in JT file is not highlighted because JT file does not 
contain precise geometry.


In the "JT Configuration" NX dialog box we should set "Include Precise Geometry"
in the "Files" tab:



In JT Configuration file  (default file is pvtrans\tessUG.config) we should set: includeBrep = true.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2016
Product: NX
Application: TRANSLATOR
Version: V1859
Function: NX_JT
Product: TC_VISUALIZATN
Application: VISVIEW
Version: V12.1.0.2
Function: 3D_FILE_JT

Ref: 001-7636503

KB Article ID# PL8010288

Contents

SummaryDetails

Associated Components