Shaded section does not display the body color for the Cut Face

2019-08-28T14:58:56Z

Summary


Details

--------------- 
In a shaded section view in drafting, the Cut Face does not display as the Body 
color, it display as a single color.



Solution

 For an existing shaded section view, select the view boundary and edit the 
view settings. Select Shading, then select the color box for Shaded Cut Face 
Color. In the Color dialog, expand the section for Selected Color and select 
the icon for Deselect All Colors --> OK --> Apply.


To set this as a default setting, open the customer defaults and go to 
Drafting --> View --> Shading tab, change the Shaded Cut Face Color setting 
from Set to Original.


This setting is a Part setting. If you use a template to create a New part in 
NX, you will need to open your template partfile and make the necessary change 
and resave the template partfile.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5
Function: DRAWING/VIEW

Ref: 001-7142482

KB Article ID# PL8010287

Contents

SummaryDetails

Associated Components