Simcenter 3D Solutions CSYS info via RMB - Information in Simulation Navigator does not match Information - Object

2020-11-10T20:46:00Z
Simcenter 3D

Summary


Details

When working in an AFEM context the RMB - Information command in the 

Simulation Navigator does not provide correct information for CSYS objects. 

The coordinate locations appear to be in the component FEM context not in the 

assembly context. How can the user view this information in the assembly 

context?

Solution

 The RMB - Information command is incorrectly listing the CSYS information in 

NX 10. This issue has been resolved in NX 11. In NX 10 the best work around is 

to use the Information - Object (Ctrl - i) command. While this command does 

list more information, it does list the correct assembly context CSYS location 

information.

Notes

KB Article ID# PL8010286

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow