Can a
CAM Parallel Generate process be started and then the displayed part be switched to a different
NX part file while it is generating? Notice In the picture below that an hour glass is displayed indicating that the operation is being generated in the background.

Solution
After the
CAM Parallel Generate routine is started in one part file the displayed part can be switched to another file. The part with the
Parallel Generate processes should not be saved, though, until the processes complete and the operations update.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1859
Function: BASIC_FUNCTIONS
Ref: 001-7606951