How to turn off the name display of specific objects

2019-05-15T15:30:13Z

Summary


Details

In Visualization Preferences, on the 'Names/Borders' tab, there is an option to 
'Show Object Names'. 
With 'Show Object Names' set to any option except 'Off', names of objects will appear in the graphical area of NX. 
However, this option turns on/off all object names. 
How can the name display of specific objects (such as solid bodies, datums, datum axis, etc.) be turned off?



Solution

 Specific object names cannot be turned off. However, if the name is removed 
from the object, then the name will not appear for that object. 
1. Open the Part Navigator. 
2. Turn OFF 'Timestamp Order'. 
 Hover the cursor over a column header, 'MouseButton3-->Timestamp Order'. 
3. Highlight the object to turn off the name display (such as solid body, 
 datum, datum axis, etc.). 
4. MouseButton3-->Properties. 
5. Select the 'General' tab. 
6. Select the 'Delete Names' ("X") button to remove the name of the object. 
7. OK the Properties dialog. 
The name has been removed for that object and will no longer display in the 
graphical area of NX.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V9.0
Function: DISPLAY

Ref: 001-7957177

KB Article ID# PL8010272

Contents

SummaryDetails

Associated Components