How to add a surface extension using Normal to Face in NX.

2019-08-28T14:58:51Z

Summary


Details

--------------- 
In NX 7.5 there are 4 options with Extension Surface, Insert --> Surface --> 
Extension:


 Tangential 
 Normal to Surface 
 Angled 
 Circular


Starting in NX 8.0, the only options under Insert --> Flange Surface --> 
Extension Surface are:


 Tangential 
 Circular


How do you create an Extension Surface by Normal to Surface?



Solution

 You can create an Extension Normal to a Surface by using the Law Extension 
function. Set the Law Types to Constant and set the Angle Law to 90 degrees.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.0
Function: FREE_FORM_MODEL

Ref: 001-7308134

KB Article ID# PL8010267

Contents

SummaryDetails

Associated Components