How do I get a blue background when I create a new part in Modeling?

2019-05-01T06:56:27Z

Summary


Details

--------------- 
Changes made in Customer Defaults -> Visualization -> Background Color, will only be honored when selecting the Blank template. 
How can I get this when selecting the Modeling template?



Solution

 1 - Create a new part.


2 - Select File -> Preferences -> Background


3 - Select Plain both for Shaded and Wireframe Views.


4 - Click on the "color" box on the right side of Plain Color


5 - Here you can select the color you want as background. On the lower right side of the window you will find Red, Green and Blue with a value in each field. These are the values you enter in "Customer Defaults > Visualization > Background Color". 
The values are from 0-255 where Red=0, Green=0 and Blue=255 gives the clearest blue color. If you would like a brighter blue you can use R=0, G=128 and B=255.


6 - Press OK twice. The background will now have the color you selected.


7 - Open the Background Color in Customer Defaults and make the changes you 
would like (see above).


8 - When you open a New part in NX you usually select a "Model" template. So 
to make your background color appear when you create a new part, this template 
has to be changed. Otherwise the new color will only appear if you select 
Blank.


9 - Make a backup copy of 
%UGII_BASE_DIR%\UGII\templates\model-plain-1-mm-template.prt


10 - Open the original file in NX and do the steps 2-7 (see above).


11 - File -> Save.


12 - Close NX and start NX again. The background should now be in your 
selected color when you create a new part file using the Model template.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1847
Function: VISUALIZATION

Ref: 001-7582397

KB Article ID# PL8010252

Contents

SummaryDetails

Associated Components