Import assembly with clone file cause relations switch back to master

2019-05-10T19:58:49Z

Summary


Details

Changed the Relationship of master model drawing from "master" to "specification", ran Dry Run to create a clone file. 
Later, executed the Import Assembly Into Teamcenter command again, and used the clone file for the import, noticed the drawing has its relation changed back to "master" again.


How to use the clone file for import and maintain that relation change to keep as "specification"?



Solution

Open the clone file in text editor, under the "Default Parameters": 

Change the parameter for "&LOG Default Naming Technique:" from
"OSFILENAME Default_Name_Rule_Type: AS_ID" to "USER_NAME". 

Save the clone file. 

Now run the Import Assembly Into Teamcenter command, use the modified clone file. The relations for drawing will remain as "specification" as was modified to initially.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: CLONE_IMPORT

Ref: 001-8950673

KB Article ID# PL8010249

Contents

SummaryDetails

Associated Components