Missing options in the Delete Face dialog

2019-05-15T16:55:50Z

Summary


Details

Select 'Insert-->Synchronous Modeling-->Delete Face'. 
The Delete Face dialog is missing two groups along with the group options. 
The Settings group in the dialog is missing along with the options: 
 Heal 
 Delete Partial Blend


The Cap Face group in the dialog is missing along with the options: 
 Cap Option 
 Select Face



Solution

 Remove the environment variable: 
 UGII_DMX_NX502=1


If this variable is set in the ugii_env.dat file: 
1. Edit the %UGII_BASE_DIR%\ugii\ugii_env.dat file in a text editor. 
2. Remove the "UGII_DMX_NX502=1" variable from the file. 
3. Save the file. 
4. Re-start NX.


If the variable is set as a system or user environment variable, following the 
instructions below for the correct operating system.


WinXP: 
1. 'Start-->Control Panel'. 
2. In the Control Panel, double-click 'System'. 
3. In the System Properties dialog, select the 'Advanced' tab. 
4. Select the 'Environment Variables' button. 
5. Find the variable "UGII_DMX_NX502=1" listed under either 
 "User variables for ..." or under "System variables". 
6. Highlight the variable: UGII_DMX_NX502=1. 
7. Select the 'Delete' button. 
8. OK the environment Variables dialog. 
9. OK the System Properties dialog. 
10. Exit the Control Panel. 
11. Re-start NX.


Win 7: 
1. 'Start-->Control Panel'. 
2. In the Control Panel, double-click 'System'. 
3. Select the 'Advanced System Settings' link on the left-hand side. 
4. In the System Properties dialog, on the 'Advanced' tab, 
 select the 'Environment Variables' button. 
5. Find the variable "UGII_DMX_NX502=1" listed under either 
 "User variables for ..." or under "System variables". 
6. Highlight the variable: UGII_DMX_NX502=1 
7. Select the 'Delete' button. 
8. OK the environment Variables dialog. 
9. OK the System Properties dialog. 
10. Exit the Control Panel. 
11. Re-start NX.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.5
Function: SYNC_MODEL

Ref: 001-6997101

KB Article ID# PL8010244

Contents

SummaryDetails

Associated Components