The dimension Arrowhead Type set in Customer Defaults are not used in Drafting

2019-08-02T11:29:15Z

Summary


Details

Setting the Customer Default for dimension Arrowhead Type to 'Closed Solid Arrow' (which has the appearance of a non-filled closed arrowhead), results in a 'Solid Arrow' (filled) being created for PMI and Drafting dimensions. (This is despite the fact that the 'Drafting - Workflow - Settings Origination' is
set to 'Drawing Standard'.)



Solution

In addition to setting the Arrowhead Type to 'Closed Solid Arrow' (via 'File --> Utilities --> Customer Defaults --> Drafting --> General/Setup --> Standard --> Customize Standard --> Common --> Line/Arrow --> Arrowhead --> Leader and Dimension --> Type'), on the same dialog it is also necessary to uncheck the 'Fill Arrowheads' option. Failing to do this will result in a 'Solid Arrow' (filled) being created, rather than a 'Closed Solid Arrow' (non-filled) arrowhead.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1872
Function: DIMENSION

Ref: 001-7857019

KB Article ID# PL8010230

Contents

SummaryDetails

Associated Components