Simcenter 3D Solutions Append Fem will not append the source fem

2019-05-08T17:29:49Z
Simcenter 3D

Summary


Details

--------------- 

When using the Append Fem... operation,(RMC on a fem in the Simulation 

Navigator), the function will not append the source fem because of the 

following error: "Source fem part open - append fem: the open fem and target 

fem abstraction types do not match". How can a user resolve the error?

Solution

 The user's target fem and source fem did not share the same solution types, 

which is a requirement of the Append Fem operation. The source fem was type 

NX Nastran Structural and the target fem was type NX Thermal/ESC. The user 

needs to change the NX Nastran Structural source fem to an NX Thermal/ESC fem 

type for the append to work properly. After making the conversion, the user 

will need to save and unload all parts in the NX session and reload the target 

fem. Once the fem's share the same type, the append function will work as 

expected.

Notes

KB Article ID# PL8010220

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow