Point selection toolbar is grayed out in Rapid Dimensioning

2019-05-13T16:18:41Z

Summary


Details

--------------- 
The Point Selection Toolbar icons are grayed out when attempting to create a 
Rapid Dimension.



Solution

 The Measurement Method in the Rapid Dimension dialog is probably set to 
Perpendicular. Set this to Inferred and the point types are now selectalble.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: DIMENSION

Ref: 001-7910325

KB Article ID# PL8010215

Contents

SummaryDetails

Associated Components