Where to find information for Spreadsheet compatibility with NX?

2019-08-28T14:58:35Z

Summary


Details

--------------- 
Where to find information for Spreadsheet compatibility with NX?



Solution

 The Information can be found in Release Notes on the GTAC Website at:


http://support.industrysoftware.automation.siemens.com/gtac.shtml


Go to; Documentation --> NX


NX8 - NX10:
----------
- Select the "NX ##" tab --> NX ## Release Notes 


- NX System Information --> NX Compatibility with Spreadsheet



NX 11;
------
- Select the "NX 11" tab --> NX 11 documentation 


- Release Notes --> NX System Information


- NX Compatibility with Spreadsheet



NX 12:
------
- Select the "NX 12" tab --> NX 12 documentation 


- Release Notes --> Open the Release Notes


- NX System Information --> NX Compatibility with Spreadsheet



NX 1800 series;
--------------
- Select the "NX 18##" tab --> NX 1872 documentation 


- Release Notes --> From Siemens PLM Doc Center


- NX System Information --> NX Compatibility with Spreadsheet




Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V8.5.3
Function: SPREADSHEET

Ref: 001-7139512

KB Article ID# PL8010208

Contents

SummaryDetails

Associated Components