Adding *New* Components are being added as Hidden.

2019-08-28T14:58:30Z

Summary


Details

--------------- 
Every time a user adds a new component to their assembly the component gets 
placed into the assembly, then it's automatically hidden.



Solution

 If a component or a set of components are set to "Show Only", this will force 
only that component or the set of components to "Always" be shown. So with 
"Show Only" being set, If the user adds a new component, it will also be 
displayed Hidden when it's added to an asssembly.


To set the "Show Only" toggle. Select any of the components in the Assembly 
Navigator and Right Mouse Button, select "Show Only", Or, Select a set of 
components and Right Mouse Button, select "Show and Hide --> Show Only"..


To remove the "Show Only" toggle. Select the Main assembly and select "Show"



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V7.5.5
Function: ASSEMBLY_MODEL

Ref: 001-6912645

KB Article ID# PL8010200

Contents

SummaryDetails

Associated Components