Usage of UGII_JT_DETAILS in NX Properties

2019-05-27T08:58:41Z

Summary


Details

--------------- 
Is it allowed to change the JT Part attribute inside the nx prt properties?


If you open a JT in NX and look to the properties of the resulting NX prt, 
there is an attribute in properties:


UGII_JT_DETAILS = 
2|1371206806|0|1|1|D:\Teamcenter11.2.2\Examples\3D\block.jt


(Example after opening the block.jt file from the TEAMCENTER VIZUALISATION 
examples folder).


Is it allowed to change this attribute to point to an ohter JT status?



Solution

 Answer from development: 
The UGII_JT_DETAILS attribute is not meant to be user modifiable.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V11.0
Function: NX_JT

Ref: 001-8320780

KB Article ID# PL8010189

Contents

SummaryDetails

Associated Components