---------------
Trim Curve is not working in NX11 (and higher) as in NX10. It is not extending the trim as
expected.
Solution
This UI was changed in NX11. The options to
Keep or
Discard in the Trim and Divide options.
When trimming a curve, the Keep/Discard option is required. The Keep is both
the original curve and the extension of the curve to be trimmed, there has to
be TWO objects selected to get the extend as intended when trimming. If only
ONE object is selected when extending by trimming, then only that object will
be the result. BOTH need to be selected when trimming with an extend intended.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V1847
Function: CURVE
Ref: 001-8805524