How to get all Cameras updated

2019-05-15T16:54:09Z

Summary


Details

When selecting different Cameras to make them active, the Cameras become 
out-of-date and they will not update again.



Solution

 It is helpful to go to 'Preferences-->Visualization', select the 
'Names/Borders' tab, and toggle on 'Show Model View Names'. OK the dialog. Now 
in the lower left side of the screen is listed the Model View name and the 
Camera that the Model View is using: 
 "Trimetric WORK Camera Trimetric".


Suppose that when the part is opened or created, the Trimetric view is the 
work view, and the Trimetric Camera is being used in the work view. 
In the lower left corner of the work view will be: 
 Trimetric WORK Camera Trimetric


In the Cameras section of the Part Navigator, double-click on "Front". 
The green check icon before "Trimetric" is replaced by the clock icon to denote 
it is out-of-date. In the lower left corner of the work view, 
will be: 
 Trimetric WORK Camera Front


The situation is that the parameters of the Front Camera have been applied to 
the Trimetric view, but the work view is still the Trimetric view, not the 
Front view. The Trimetric Camera is still linked to the Trimetric view, but 
the data being shown in the Trimetric view is no longer that of the Trimetric 
Camera. In this situation, the Trimetric camera is out-of-date, because what 
is seen in the Trimetric view is no longer the same as the parameters of the 
Trimetric Camera.


The following will correct the situation: 
1. For the Camera that is out of date, make the corresponding 
 Model View active. 
2. Then highlight the corresponding out-of-date Camera, 
 'MouseButton3-->Activate'. 
3. For the next camera that is out of date, repeat steps 1 and 2 until all 
 the Cameras are activated in their corresponding Model View.


For example, if the "Right" and "Top" Cameras are out of date: 
Make the "Right" Model View active, then select the "Right" Camera, 
'MouseButton3-->Activate'. Make the "Top" Model View active, then select the 
"Top" Camera, 'MouseButton3-->Activate'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V9.0.3
Function: VISUALIZATION

Ref: 001-7591859

KB Article ID# PL8010183

Contents

SummaryDetails

Associated Components