Option to let user individually set thier own user interface environment

2019-05-15T16:51:13Z

Summary


Details

Currently, all users are using the 'Classic Layout', but some users want to 
use the 'Ribbon Bar'. How can this option be set individually so users can 
choose their own User Interface Environment?



Solution

 The Customer Default 'User Interface Environment' controls whether there is a 
user preference. If a site has this set to either 'Classic Toolbars Only' or 
'Ribbon Bar Only', then users are unable to set this option individually in 
the user preferences. This option in Customer Defaults needs to be set to 'User 
Preference' in order for the option to appear in the User Interface Preferences 
and allow users to set this individually.


In order for users to have this preference available, please follow these 
instructions: 
1. In Customer Defaults, expand 'Gateway' and highlight 'User Interface'. 
2. Select the 'Layout' tab. 
3. Set the User Interface Environment option to 'User Preference'. 
4. OK the Customer Defaults dialog. 
5. Re-start NX.


When 'User Preference' is set, then users can choose their layout in 
Preferences. 
1. Select 'Preferences-->User Interface'. 
2. Select the 'Layout' tab. 
3. Set the User Interface Environment to the preferred option, 
 'Ribbon Bar' or 'Class Toolbars'. 
4. OK the User Interface Preferences.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V9.0
Function: PREFERENCES

Ref: 001-7524712

KB Article ID# PL8010179

Contents

SummaryDetails

Associated Components