Deleting an Ordinate Origin with no name display in NX9

2019-08-28T14:58:05Z

Summary


Details

--------------- 
Cannot delete an Ordinate Origin with no name displayed in NX9. How can you 
turn on the Ordinate Origin name so that it can be deleted?



Solution

 Double-click on one of the Ordinate Dimensions, this will display the Ordinate 
Origin symbol (Orange square symbol). Select the Ordinate Origin symbol and 
the Ordinate Origin shortcut menu opens. Select the Ordinate Set Settings 
button.


From the Settings dialog, select Ordinate. In the Origin Symbol section of 
the dialog change the Display Name Style from None to Ordinate Set Name, 
Close the Setting dialog, and the Ordinate Dimension dialog.


Select the Ordinate set Name --> Right mouse button --> Delete.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DIMENSION

Ref: 001-7127306

KB Article ID# PL8010172

Contents

SummaryDetails

Associated Components