NX Is Cloud-based licensing available for NX?

2019-05-10T14:30:38Z
NX System Administration

Summary


Details

Is Cloud-based licensing available for NX?



Solution

The most recent version of SPLM Licensing is CAPABLE of supporting Cloud-based 
licensing, however the NX application has not implemented this feature. 
Siemens PLM is investigating Cloud-based licensing, but nothing has been 
announced or released. 


There is another option for supporting remote licensing.


You can set up a VPN connection between the license server and the client.This 
would allow the client to accesss the license server at both the server 
location and at the remote location.


The VPN connection would need to allow TCP port traffic on both port 28000 and 
the dynamic port used by the vendor daemon 'ugslmd.exe'. The dynamic port for 
the vendor daemon can be made static by editing the VENDOR line in the license 
file and adding the 'PORT' variable. For example, if you want to set the 
VENDOR daemon to use port 28001, the VENDOR line in the license file would 
look like, 


 VENDOR ugslmd PORT=28001



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1859
Function: WNT_OS_ISSUES

Ref: 001-7800778

KB Article ID# PL8010167

Contents

SummaryDetails

Associated Components

Installation