The 'Move Component' command displays X,Y,Z pop-up

2019-05-15T15:29:02Z

Summary


Details

When using the 'Move Component' command, an X,Y,Z pop-up displays in the work 
area and is hiding portions of the assembly.



Solution

 Select F3 in order to disable the display of the XYZ input. 
Selecting F3 two more times will return the display of the XYZ input field.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: POSITIONING

Ref: 001-7574760

KB Article ID# PL8010163

Contents

SummaryDetails

Associated Components