-----------
PROBLEM
-------
Tc11.2.1 and NX 10.0.3.5
One user is unable to start NX from Teamcenter.
ugraf.exe crashes.
Solution
- tcserver syslog shows:
bulk_check_privilege called on bad tag 00000000 with invalid DM
bulk_check_privilege called on bad tag 00000000 with invalid DM
515001 - BusinessObjectRegistryImpl::askObjectTypeInfo failed
- ugs_router syslog shows :
>>>> Error code 3070023 caught in file
"D:\workdir\reference\NX1003_5\src\interop\no\ind\interop_socket_writer_definit
ions.c" at line number 797
>>>> Error code 3070023 caught in file
"D:\workdir\reference\NX1003_5\src\noug\no\ind\launcher_main.c" at line number
1054
@@@ End of session Wed Aug 17 23:00:16 2016 Eastern Daylight Time
When user tried to create a folder under home folder within temacenter,
he got this message:
"you may not remove the mail folder from a home folder"
Seems like a corrupted home space.
Ran reset_user_home_folder.exe
That fixed corrupted home folder issue. Once that was fixed, NX started up from
Teamcenter without any problems.
Notes