NX There is an error when exporting an IGES file, 'no parts in current input file'

2019-05-15T15:28:58Z
NX for Design

Summary


Details

The following error is displayed while exporting an IGES file: 
 no parts in current input file



Solution

 Verify that the IGES file name, including the names in the folder path, do not 
contain a comma (,).


The comma character is not allowed in a folder name or file name during the 
process of exporting or importing files. 
The reason is that NX uses the comma character to separate and filter files to be processed through the .def file.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V7.5
Function: IGES

Ref: 001-7218775

KB Article ID# PL8010160

Contents

SummaryDetails

Associated Components

CAD Translators