Extract curves from a split body and send to a sketch

2019-05-15T15:28:53Z

Summary


Details

Customer had a model with a split body and wanted to extract the cross sectional edge curves and send them to a sketch.



Solution

Here is how to accomplish the task:


1.  With the desired portion of the split body exposed, select Menu -> 
     Insert -> Derived Curve -> Extract Curve


2.  Select Edge Curves from the dialog box, then select 'All in Face' and 
     select the faces with the desired curves and click OK, then OK again 
     and cancel from the dialog box


3.  Now, the curves need to be projected onto the desired plane for the 
     sketch that will be later added. Add the datum plane for the sketch if 
     one is not existing at this point


4. Under the Curve tab, select Project Curve (Menu -> Insert -> Derived 
 Curve -> Project Curve) and select the curves to be projected


5.  Under 'Select Object' in the dialog, select the datum plane that the 
     sketch will be placed on


6.  Under 'Specify Vector' select the appropriate direction/vector (normal 
     in this case) for projection. Note: The curves must NOT be 
     associative because they will be added to a sketch, so be sure that the 
     'Associative' box is unchecked under 'Settings'(sketches cannot have 
     parents, only children) and click OK


7.  Start 'Sketch in Task Environment and select the sketch plane and close 
     the 'Profile' dialog if it has popped up


9.  Use the 'Add Existing Curves' (Menu -> Insert -> Curve from Curves -> 
     Existing Curves) and select the projected curves


10.  The curves are now added and a part of the active sketch


Note:  View Section/Edit Section can also be used to extract the cross 
            sectional curves by using the option under Section Curve Settings 'Save 
            Copy of Section Curves'



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V11.0.2
Function: SKETCHER

Ref: 001-8953699

KB Article ID# PL8010156

Contents

SummaryDetails

Associated Components