Auto Fit every time a component is turned on or off

2019-05-15T16:49:56Z

Summary


Details

Every time a component in the assembly is hidden or shown, the graphics area 
will perform an automatic 'Fit' operation. How can this be prevented so the 
current zoom factor is not lost when components are hidden or shown?



Solution

 The following setting controls this behavior: 
1. In the Menu, select 'Preferences-->Visualization'. 
2. Select the 'View/Screen' tab. 
3. Turn off the setting 'Fit on Show or Hide'. 
4. OK the Visualization Preferences dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: ASSEMBLY_MODEL

Ref: 001-7465105

KB Article ID# PL8010132

Contents

SummaryDetails

Associated Components