Array a component in a hole pattern

2019-05-08T19:36:36Z

Summary


Details

--------------- 
How can you array a component in a hole pattern similar the the past Feature 
Iset function?



Solution

 Create the hole pattern desired at the component level. Return to the assembly level and add an occurrence of the hardware placing in in the first hole of the pattern.


After placing the initial object (i.e., bolt, etc) select Assemblies --> Components --> Pattern Component --> select Reference from the Pattern Type dropdown.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: ASSEMBLY_MODEL

Ref: 001-6904113

KB Article ID# PL8010128

Contents

SummaryDetails

Associated Components