Simcenter 3D Solutions Polygone Edges are being merged when creating mesh.

2019-09-13T07:19:08Z
Simcenter 3D

Summary


Details

After creating a 2D mesh, all polygon edges are merged . The single edges as they were, are no longer selectable. Only one or 2 "long" edges are left to select. Why does this happen and can this be undone.

Solution

Edit the 2D mesh. If necessary, unfold the menu area "Model Cleanup Options ".

Here you will find the option: "Merge Edges ". Uncheck this option and press OK.

(Make sure the original geometry/part is loaded). 

Now the mesh will be updated, and the polygon edges are no longer merged.

Notes

KB Article ID# PL8010126

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow