Adding PMI to an Assembly Sequence

2019-05-15T16:48:37Z

Summary


Details

How to add PMI to an Assembly Sequence.



Solution

 Assembly Sequence has already been created: 
1. Go to the Modeling application. 
 If currently in the Assembly Sequence application, select 'Finish' to 
 enter the Modeling application. 
2. In the Part Navigator, expand 'Model Views'. 
3. Highlight 'SEQUENCE_VIEW', 'MouseButton3-->Make Work View'. 
4. While in the Assembly Sequence model view, create the PMI that is needed. 
 If PMI already exists... 
 a. In the Part Navigator, expand 'Model Views'. 
 b. Expand the Model View that contains the existing PMI. 
 c. Highlight the existing PMI, 'Mousebutton3-->Display-->in Views'. 
 d. Toggle ON, 'SEQUENCE_VIEW'. 
 e. OK the Display in Views dialog. 
5. Select the 'Sequence' icon to enter the Assembly Sequence application. 
The PMI is now available in the Assembly Sequence.


Assembly Sequence has not already been created: 
1. Select the 'Sequence' icon to enter the Assembly Sequence application. 
2. Select the 'New' icon to create a new Sequence. 
3. Select the 'Finish' icon to exit the Assembly Sequence application. 
4. Continue with the above steps defined in, 
 "Assembly Sequence has already been created".



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: SEQUENCING

Ref: 001-7611575

KB Article ID# PL8010125

Contents

SummaryDetails

Associated Components