How to permanently set the B-Spline tolerance in the STEP translator

2019-05-15T15:28:24Z

Summary


Details

How to permanently set the STEP214 translator B-Spline tolerance to the minimum metric tolerance for B-Spline data.



Solution

1.  Open the following file in a text editor: 
     %UGII_BASE_DIR%\STEP214UG\ugstep214.def 

2.  In the file, find the following option and set it to the following value: 
     PA_EDGE_FACE_BSPLINE_APPROX_TOL = 0.0000101 

     NOTE: This is in millimeters. 

3.  Save the file. Exit the Text Editor.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V10.0.3
Function: STEP_AP214

Ref: 001-8945765

KB Article ID# PL8010123

Contents

SummaryDetails

Associated Components