How to control the placement of the dimension text between the extension lines

2019-05-15T15:28:15Z

Summary


Details

How to control the placement of the dimension text between the extension lines.



Solution

 1. During the creation of the dimension, expand the Settings group in the 
dialog. 
2. Select the 'Settings' icon. 
3. In the Settings dialog, expand 'Line/Arrow' and highlight 'Arrowhead'. 
4. Under the Workflow group, toggle off 'Automatic Orientation'. 
5. Close the Settings dialog.


Now when placing and locating the dimension, the text can be located between 
the extension lines left or right (with horizontal dimension) or up and down 
(with vertical dimensions).



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DIMENSION

Ref: 001-7248588

KB Article ID# PL8010120

Contents

SummaryDetails

Associated Components