NX Deformable part result in an assembly level body when doing NX to STEP export.

2020-04-29T08:39:59Z
NX for Design

Summary


Details

Have an assembly with 3 components. Two of the components are deformable parts, so in the assembly there exists 2 deform part features. One of the deformable parts are suppressed through arrangements.


The assembly is translated from NX to STEP using AP203, (or AP214). The resulting STEP file contains just one deformable part component, which is correct as the other was suppressed through arrangements. 
BUT, both the deformable parts bodies show up in the STEP assembly. After a closer examination the remaining deformable part component is empty and there are 2 bodies in the assembly itself.


How to translate an assembly like this and get the expected result, i.e. one deformable part component with one body inside?



Solution

 The NX to STEP AP203 and AP214 translators are not designed to handle a situation like this. The deformable part features in the assembly itself is interpreted as the body representations, the deformable part components are subsequently considered to be empty and the suppression of one of the components is therefore not taken into account with respect to the bodies, only with respect to the component.


The solution is to use the STEP AP242 translator . This translator honors the special characteristics of a deformable part and processes them accordingly. 
Please note that the STEP AP242 translator is a separate product, i.e. requires a specific license.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: TRANSLATOR
Version: V1899
Function: STEP_AP242

Ref: 001-8824659

KB Article ID# PL8010119

Contents

SummaryDetails

Associated Components

CAD Translators