Simcenter 3D Solutions Exporting SIM files from NXManager

2019-05-07T17:28:14Z
Simcenter 3D

Summary


Details

--------------- 

How can I export a sim file out of teamcenter using the ugmanager_clone 

utility?

Solution

 To export a sim file out of Teamcenter using ugmanager_clone, use the 

following switches (using 000077.sim1 as an example below):

ugmanager_clone 

-pim=yes 

-u=infodba 

-p=infodba 

-o=export 

-asse=@DB/000077.sim1/A/cae_solution<mailto:-asse=@DB/000077.sim1/A/cae_solutio 

n> 

-default_n=autotranslate 

-default_d=C:\temp\export 

-s=C:\temp\export\export.log

ugmanager_clone -help gives explanations of the above switches.

The following files were exported/created in C:\temp\export\

000077.fem1_A.fem 

000077.i1_A.prt 

000077.sim1_A.sim 

000077_A.prt 

export.log

Note that replacing -asse with -par only exports the sim:

-par=@DB/000077.sim1/A/cae_solution<mailto:-par=@DB/000077.sim1/A/cae_solution>

000077.sim1_A.sim 

export.log

If you also want the drawings (specifications or manifestations) add the 

following switch:

-copy_n=specification:yes or -copy_n=manifestation:yes

C:\apps\CAD\NX10.0\UGII>%UGII_BASE_DIR%\ugmanager\ugmanager_clone -pim=yes 

-u=infodba -p=infodba -o=export 

-asse=@DB/000077.sim1/A/cae_solution<mailto:-asse=@DB/000077.sim1/A/cae_solutio 

n> -default_n=autotranslate -copy_n=specification:yes 

-default_d=C:\temp\export -s=C:\temp\export\export.log

Notes

KB Article ID# PL8010110

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow