Sketch constraint symbols do not display, but do list in the geometric constraint

2019-08-28T14:58:01Z

Summary


Details

--------------- 
In a case where a sketch has 2 horizontal lines and a verticle at the 
Mid-Point of each line, it will display the midpoint constraint symbol. Adding 
a Collinear constraint will cause the 2 lines to be positioned on top of each 
other. Now the MidPoint constraint no longer displays graphically or in the 
Quick Pick menu. But it still shows in the Show/Remove Constraints menu. Why 
doesn't it display?



Solution

 After adding the collinear constraint, the verticle line that was between the 
reference edge and horizontal line still exist, but is very small. In fact, it 
is a zero length line, but it still exist. The symbol will not display with 
small geometry.


There is a Sketch Preference setting called "Dynamic Sketch Display" if toggled 
OFF, then the symbols will display. So, while in the sketch, go to Menu --> 
Preferences --> Sketch --> Session Settings (tab) --> Dynamic Sketch Display.


Here is the documentation on the Dynamic Sketch Display;


Go to;


 CAD --> Sketching --> Sketch Preferences: what do you want to do?


Dynamic Sketch Display 
====================== 
When this option is selected, constraint and vertex symbols do not display if 
the associated geometry is very small. To see these sketch objects regardless 
of associated geometry size, clear this check box.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V10.0
Function: SKETCHER

Ref: 001-7713191

KB Article ID# PL8010109

Contents

SummaryDetails

Associated Components