Datum planes do not display as translucent.

2019-05-15T15:28:10Z

Summary


Details

Datum planes do not display as translucent.



Solution

 To display datum planes as translucent, perform the following: 
1. Select 'Preferences-->Visualization Performance'. 
2. Select the 'General' tab. 
3. Uncheck 'Disable Plane Translucency' option. 
4. OK the Visualization Performance Preferences dialog. 
Now all datum planes will display as translucent. 
Note: This does not apply to a Datum Csys.


This can also be set in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Gateway' and highlight 'Visualization'. 
3. Select the 'Performance' tab. 
4. Under the General Graphics area uncheck 'Disable Plane Translucency'. 
5. OK the Customer Defaults dialog. 
6. Restart NX to have the new settings take effect.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V7.5
Function: DISPLAY

Ref: 001-6871908

KB Article ID# PL8010107

Contents

SummaryDetails

Associated Components