Create Linked Mirror Part plane is not associative

2019-05-15T16:46:32Z

Summary


Details

When editing or modifying the orientation of the plane used to create the 
Linked Mirrored Part, the mirrored part does not update to the new location. 
Isn't the plane selected for the 'Create Linked Mirror Part' associative?



Solution

 NX does not allow the editing of parameters for the 'Create Linked Mirror 
Part' operation (ie., editing to select a different reference set to copy, or 
selecting a different plane for mirroring). Also, the plane selected for the 
Mirrored Part is fixed. The mirror plane is not associative to the source part 
plane. The selection of the mirror plane in the work part is simply to define a 
location for the non-associative mirror plane.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.5
Function: FEATURE_MODEL

Ref: 001-7912087

KB Article ID# PL8010106

Contents

SummaryDetails

Associated Components