NX ISV - Machine Configurator Licenses

2019-10-18T08:36:19Z

Summary


Details

---------------

For NX IS&V, which NX Machine Configurator license is required?

NX32405 NX Machine Configurator Basic 

NX32406 NX Machine Configurator Advanced

Solution

With the Basic license the controller functionality is limited to what is provided by the CCF-File.

The Advanced license allows use of an XML-based configuration language to define sophisticated machine behaviors.

'Basic' is mostly limited to use our OOTB examples and reconfigure to the customized machines.

If the machine does not fit to any of the OOTB Kinematic Types or if there are more functions available inside the controller that we do not support inside OOTB example, then 'Advanced' is required.

Notes

KB Article ID# PL8010105

Contents

SummaryDetails

Associated Components