---------------
Need to convert an Abaqus fem to an NX Thermal
Solution
In order to convert a FEM model from one solver to another start by using right
mouse button on the name of the FEM at the top of the simulation navigator and
select edit. On the edit form you can change the solver type.
After changing the solver many of the meshes will become "inactive". This is
because the element properties for the new solver are different than the
properties for the original solver.
Starting in NX 10.0, the way to remove the inactive flag from the meshes is to
use edit, element, modify type. On the modify type form you have the option of
converting the original collector or creating a new collector.
Notes